Resources

Filter by

Knowledge is power when it comes to high voltage

High voltage capabilities help solve a range of design challenges for some of the world's most impactful technology. Des...

Blog Posts

Understanding power supply de-rating specifications

An increasing number of AC-DC power supplies rely on de-rating specifications. But what exactly are they? Read our lates...

Blog Posts

When are configurable power supplies the best option?

Configurable power supplies allow you to tailor the output voltage, number of outputs and current levels to your specifi...

Blog Posts

Achieving both precision and accuracy in high voltage power applications

Our blog discusses why achieving both precision and accuracy in high voltage DC power supplies can be tricky for designe...

Blog Posts

What is surge testing and why is it important?

Discover why surge testing is vital for making sure equipment is protected from unexpected voltage spikes or power surge...

Blog Posts

How to integrate high voltage in advanced manufacturing applications

How do manufacturing companies stay one step ahead of the field? Advanced manufacturing methods are helping companies ga...

Blog Posts

Powering high voltage detector solutions with speed, accuracy and reliability

Detectors are a critical part of analytical equipment used in semiconductor inspection, medical imaging, and mass spectr...

Blog Posts

New baseplate cooled AC-DC power supply delivers complete solution for rugged applications with limited or no airflow

Announcing the launch of a new series of low profile, baseplate cooled 160W AC-DC power solutions.

News

Selecting the best AC-DC power supply for peak load applications

If specified correctly, dual rated power supplies perform strongly in high peak power applications. All you need to know...

Blog Posts

What are electrostatic chuck power supplies?

Electrostatic chucks are used for a wide range of power applications. They are vital for semiconductor manufacturing as...

Blog Posts

High voltage power supplies explained

High voltage power supplies are specialized electrical devices that creates voltages typically above 1,000V.

Blog Posts

Electrolytic capacitors determine the lifetime of a power supply

The service life of electrolytic capacitors is a key design parameter in power supplies. Our blog summarises the manufac...

Blog Posts